Cancel
Showing results for 
Search instead for 
Did you mean: 

Pulling Parts from a Store Using Flow Control

Hi All,

 

I am trying to model a system that includes buffers that can hold multiple variations of parts. So Product A & Product B (made on different production lines) can both be stored in the same buffer. These parts, along with several others, are then pulled by the next processor in a sequenced order (currently by using FlowControl dictated by predecessor order).

 

I am struggling to figure out how to have multiple parts stored in a single buffer (or store) but still be able to pulled through to the next processor in sequence (Example, Pulling Processor wants Product B as next part in sequence however the next part in the Buffer in Product A, how can I make so Product B is still pulled?).

 

There is probably an easy solution to this but I cannot get my head round it!

 

Thank you for any possible help you can provide.

 

Kind Regards,

 

Nathan

5 REPLIES 5
Highlighted

Re: Pulling Parts from a Store Using Flow Control

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Nathan,

since the Buffer has only two types (Queue and Stack) the parts can not overtake.

The object Sorter is a buffer with can change the sequence of parts.

In the Example models (item Small Examples) there is a model with an optimization of the sequence of the buffer. Category Tools and Optimization, Topic Optimization in the Sim. The sequence is determined by an userdefined attribute SortCriteria.

Maybe you use the name of the parts "ProductA" and "ProductB". Before you take a part you call

Sorter.sort;

Since the parts must be able to overtake you can also use the object ParallelProc. In an exit control you can scan the contents of the ParallelProc and you can determine the right next part.

Furthermore there is an example with the pull control: Category Material Flow Topic Pull Control, Example Color sorting buffer.

Regards,

Peter

 

Re: Pulling Parts from a Store Using Flow Control

Siemens Phenom Siemens Phenom
Siemens Phenom
You will have to implement a kind of warehouse management system that allows you to access the stored parts. How complex this WMS is going to be depends on many aspects. Assumed each part occupies the same space in the store it could be an idea to build the store as a frame containing as much buffers as you have different parts. Each part moves into its dedicated buffer (capacity=-1), so pulling a part just requires to access the right buffer. One thing of course has to be considered, this is the total capacity of your warehouse. For that just introduce a counter or use WarehouseFrame.numMU.

Regards

Always consider using the AttributeExplorer!

Re: Pulling Parts from a Store Using Flow Control

Hi Peter,

 

Thank you for your response. Unfotunately I am still having issues with this.

 

I think Parallel Processors may be the way forward with this, however I am not sure how you scan the ParallelProc to determine the next right part like you mentioned. Do you have any tips on this? Thanks again for any help you can give.

 

Kind Regards,

 

Nathan

Re: Pulling Parts from a Store Using Flow Control

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Nathan,

by the fllowing loop you can consider all MUs which are on a station ParallelProc:

local MUobj:object;
for local j := ParallelProc.numMU downto 1 loop
  MUobj := ParallelProc.MU(j);
  if MUobj.ID = 3 then
MUobj.move(SingleProc);
  end;
next;

Maybe you will call this loop when a MU arrives. In this case you prepare an Entrance control of the ParallelProc.

Regards,

Peter

Re: Pulling Parts from a Store Using Flow Control

Thanks Peter, really appreciate your help!

Kind Regards,

Nathan