Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Question: Change production in a source object.

Experimenter
Experimenter

Hi everyone,

I'm starting to learn how to use Plant Simulator and I have a very basic question for which I cannot find an answer yet.

I'd like to set the production rate of a source object to "MU/hour", for instance 7 MU/hour or a normal distribution of 20 mu and 5 sigma MU/hour. I think I can only set the production time interval, but that is not what I'm looking for. Do I have to do it through a method?

 

Thanks for your responses.

2 REPLIES 2

Re: Question: Change production in a source object.

Phenom
Phenom

You can set a constant production rate 

 

In your case of 7 mu/hour  this would mean

 

3600 : 7 = 514.3 sec interval.

 

or

 

you can select /set a distribution.

 

or 

 

you can create a formula (s. fig2 , below)

 

or 

 

you can calculate the interval by a method 

 

e.g. source.intervall :=3600.0/7.0

 

 

Check the dropdown list between interval and interval value

 

Unbenannt1.PNG

Re: Question: Change production in a source object.

Experimenter
Experimenter

Thanks for your response,

 

It seems that's the only way to do what I need to do. I thought you could just set the production ratio in MU's/hour instead of doing all the math (which could introduce some rounding errors) or coding a method to calculate the time interval.