Cancel
Showing results for 
Search instead for 
Did you mean: 

Questions about tables

Dear community,

 

2 simple questions about the table:

 

1) Is there any way to higlight the content of a cell? i've to compare two times and if one is low than the other i need a green cell, otherwise in red. i've tried to search "highlight" and "table" in forum and help but nothing came out.

2) Is there any way to erase permanently the unused row and column of a table? if i just want, for example, a table of 2 columns and 10 row how can i erase the other ones?

It's not fundamental but it seems strange to me that it is not possible.

Thanks for the help.

1 REPLY

Re: Questions about tables

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
1) setBackgroundColorCells or context menu in the cell --> format

2) to restrict the table you can use the attributes maxXDim and maxYDim (doubleclick it in the attributes window and set the values there)
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net