Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Random number streams student license

Experimenter
Experimenter

When I choose a distribution, like in this case the Normal distribution for the set-up time, the program does'nt asks for the stream. When we are using the schools computers the program asks for it so I wonder if there are some setting that I can change to make it ask for the stream? Or does'nt it work in the student license?

 

Thanks in advance.

 

2 REPLIES 2

Re: Random number streams student license

Siemens Phenom Siemens Phenom
Siemens Phenom

In V11 you no longer have to manage the random number streams manually. Each object gets it's individual stream assigned and is therefore independant from the other objects.

 

If you want to get more detail just select "New Features" on the start page.

It will open the online manual with a description of the new featrures in V11.

Here select "Eminent Changes in Plant Simulation 11".

The second item then describes the changes.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Random number streams student license

Experimenter
Experimenter
Thank you for the quick response!