Cancel
Showing results for 
Search instead for 
Did you mean: 

Re-schedule event in the event list

Creator
Creator
Hello everybody, I'm looking for a Simtalk command which allow to modify the time of an event in the list of Event Debugger. Does it exists such command for re-scheduling an event (later of course). Thanks,
5 REPLIES 5

Re: Re-schedule event in the event list

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Jer_N,

 

When you want to reschedule methcalls, it is possible. First you kill the current event with deleteMethcall and then schedule the new event.

 

If this is not your issue, please specify your problem more clearly.

 

Regards,

Gert Nomden


Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com

Re: Re-schedule event in the event list

Creator
Creator
Hi, It's not for my own events but default event planified by the software. For example, I put a cycle time for a set-up, so the event "SetUpEnd" is planified. If I want to modify the time of this event "SetUpEnd" , is it possible ? Regards,
Highlighted

Re: Re-schedule event in the event list

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Hi Jer_N,

 

The SetupEnd depends on several factors. But the duration of the setup becomes a given once set-up is initiated. The software may reschedule it, for instance, if a resources (e.g. Worker) that is required for the set-up gets interrupted. But what you do is you just interrup it. The software remembers the remaining set-up time and schedule the event accordingly.

 

I don't know what you mean by "cycle time for a set-up".

 

It helps if you explain what kind of system you are working on and what you try to achieve there. In many cases this kind of detail control has little impact on the overall performance, so we stick to the default behaviors.

 

Regards,

Gert


Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com

Re: Re-schedule event in the event list

Siemens Phenom Siemens Phenom
Siemens Phenom

You can use the method 'endSetupIn' to achieve this.

_________________________________________________________________
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Re-schedule event in the event list

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Ouch!

 

Never thought of this. And it works both ways, so you can postpone the completion of the set-up!

 

Thanks to MichaelJoos...


Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com