Cancel
Showing results for 
Search instead for 
Did you mean: 

Read range from excel

Legend
Legend

Hello All,

 

Can we read range from excel and text file((like from (1,7)...(.,.)) and write it in table file but from (0,7) like that not from (0,1).

in that tablefile, i activate column index.

Is it possible. Can you suggest code for that. its very difficult to find in help.

 

Thanks in advance

1 REPLY 1

Re: Read range from excel

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

you can have a look at the attached model as a starting point for that. In this model data is read from and written into an excel file in Plant Simulation using ActiveX. In the method object "GetDataFromInput" you can specify the source range from your excel file and the target range in your table.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution