Cancel
Showing results for 
Search instead for 
Did you mean: 

Real Time Production & Data Importation

Experimenter
Experimenter

Hi everyone.

i have some questions, the answers will help me on my project.

 

1- Is it possible to simulate production in real time with the real production system? 

2- If i want to place a machine, what data i need to import from the production system ?

 

Thank you.

6 REPLIES 6

Re: Real Time Production & Data Importation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
What do you mean with " the real production system" ?

Have a look into the Dialog of the Station / SingleProc. Here you find the data-set you need to import (+ failure data).
In addition to this you need the position of the machine, associated buffers, all Information about the materialflow (predecessor - successor) for each kind of part, maintenance information...

Using one of the data Interfaces, you can share information with the production system.
Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Real Time Production & Data Importation

Valued Contributor
Valued Contributor
你做实时仿真吗

Re: Real Time Production & Data Importation

Experimenter
Experimenter
Thank you Mr. Steffan for your time, and for your precious answers.
What i meant by "The Real Production System" is the connection between what happens in the industrial field and the Plant Simulation in real time, it's kind of supervisory of the production system.

Re: Real Time Production & Data Importation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You can quite easily exchange "live" data through the OPC-interface.


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com

Re: Real Time Production & Data Importation

Valued Contributor
Valued Contributor
dear Nomden
do you have a example that exchange "live" data between plant and mes system,thank you

Re: Real Time Production & Data Importation

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

No, sorry, simply because you need more than just an spp-file. But if you master a bit of SimTalk it is quite easy to set up. You need to make a mapping between your model and your MES, for both objects and attributes. I would suggest to create a small test environment with a small model, OPC server and MES.


Gert Nomden
Senior Consultant | Tecnomatix Product Manager
cardsplmsolutions.com