Cancel
Showing results for 
Search instead for 
Did you mean: 

Real decimal places in Table issue

Creator
Creator

Hi,

 

I have an issue with only being able to use two decimal places in my real columns:

s1.PNG

In the above example 2000/86400 is rounded to 0.02 (more close is 0.023)

 

If I try to manually put three decimals I get format error:

s2.PNG

 

I have looked in settings and searched the forum to no avail.

What is the solution?

 

Thanks in advance

1 REPLY 1
Highlighted

Re: Real decimal places in Table issue

Phenom
Phenom

The solution is :

 

1. select column

2. press right mouse button

3. select format

4. select last tag ( data type)

5. change format