Cancel
Showing results for 
Search instead for 
Did you mean: 

Recording Order of Parts Passing Through a Processor

Hi Everyone,

 

I was wondering if anyone could help me! I'm looking to record the parts that pass through a single processor (Paint_Pull) into a Table File. I would like the part name to be recorded on entry to the processor and index down as each part passes through.

 

Thanks for any help!

 

Kind Regards,

Nathan

5 REPLIES 5

Re: Recording Order of Parts Passing Through a Processor

Phenom
Phenom

you mean something like this ?

 

Unbenannt.png

 

Re: Recording Order of Parts Passing Through a Processor

Solution Partner Creator Solution Partner Creator
Solution Partner Creator

You can do that with a TimeSequence Object and the recording method is not required.

 

Smiley Tongue

 

Just the reset one cleaning the table.

Re: Recording Order of Parts Passing Through a Processor

That looks like what I would need from the image, however I'm running 11.2 so can't open the simulation!

Re: Recording Order of Parts Passing Through a Processor

Thanks, I'll have a look into this as I have never used that object before!

Re: Recording Order of Parts Passing Through a Processor

Is there any chance you could re upload this simulation so I can view it in 11.2 please?