Cancel
Showing results for 
Search instead for 
Did you mean: 

Regarding utilization of all resources of machine during simulation

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello everyone,

 

I am currently working on a project which requires considerable amount of CPU resources during simulation. I am using a 16GB ram machine. However, by observing task manager during simulation, i have realised that, all the machine resources are not utilised duing simulation. Is there any way to increase the resource utilisation.

 

I have attached the machine specifications and also resource monitor snapshot.

 

Thanks in advance

1 REPLY

Re: Regarding utilization of all resources of machine during simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi learner,

 

a single simulation run can only utilize one core of your computer.

If your taskmanager shows 8 CPUs you only will have an utilization of 15%.

 

But usually you have to do various simulation runs with different input parameters and with different seed values.

 

The experiment manager gives you the ability to distribute these simulation runs.

So each simulation can either run in another process on your machine or even on a remote machine.

 

This way you can get a higher utilization.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.