Cancel
Showing results for 
Search instead for 
Did you mean: 

Removal of entities

Pioneer
Pioneer

Attached is the model in which parts are removed from the line one by one while other parts get entered. I need assistance that all 25 parts get removed at once from dryer1 and other 25 parts get in and wait fo 30 mintues. Same with dryer 2. 

Kindly Help.

4 REPLIES

Re: Removal of entities

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

do you want to have the dryer complete empty, before you fill it anew?

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Removal of entities

Pioneer
Pioneer

yes.

Re: Removal of entities

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

where you want to collect the members of the charge: inside or outside of the dryer (in the case of a dryer or a batch processing it is very uncommon to collect the batch inside of the equipment), if you want to collect outside, then you need for each dryer a buffer.

 

The buffer you can equip with an exit-lock, which opens, if the dryer is complete empty and the buffer has the right number of parts.

An entrance lock in the buffer you can use to collect the right number of parts. The dryer then only needs to stop (near the exit) and wait for the processing time.

 

If you want to collect inside the dryer, you can also use the exit and the entrance lock.

If the dryer is empty (and at the beginning of the simulation) you lock the exit. In the entrance control of the dryer you count the parts, close the entrance if there are enough parts in the dryer and open the exit after the processing time...

In the exit control (rear) you open the entrance, if the equipment is complete empty...

 

This is a good example for a starter.

 

SimTalk: entranceLocked, exitLocked, numMu, wait --> see help

 

But it is your job to create the model...

 

 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: Removal of entities

Pioneer
Pioneer

Attached is the snap shot, what I really want is to pass entities from each of line at once respectvely to another attached line. For that kindly help me out.