Cancel
Showing results for 
Search instead for 
Did you mean: 

Replicate Results Consistently

Experimenter
Experimenter

Hello All,

 

I am trying to run my simulation with the same paramenters and obtain the same results each time to determine the effect of changing specific values.

My input sources are writing off a table and do not change on a reset.

My random numbers variant is 1 and it does not increment on reset. I'm unsure of the effect of antithetic numbers but I have tried it both with and without. Also, I only have 1 as a random seed value.

Is there a setting or value that needs to be changed to obtain identical results?

If it is one of the parameters above it may be an overlooked portion in my simulation, but I don't think so.

 

Thanks in advance.

 

2 REPLIES 2

Re: Replicate Results Consistently

Phenom
Phenom

settings should look like this

 

Unbenannt1.png

Highlighted

Re: Replicate Results Consistently

Experimenter
Experimenter

That is what I have.

Could there be another random process or setting? Or does it lie in my simulation?

 

Thanks