Cancel
Showing results for 
Search instead for 
Did you mean: 

Request for a column autoadjust feature in PlantSimulation

Builder
Builder

Hi!

 

When working with tables and lists, I am often suffering from being misleaded by the fixed default colum width dimension of 20 units hiding further information written in the table cells.

 

May I ask if a certain "autoadjust" feature can be implemented in future versions of PlantSimulation which are adjusting the column width according to the longest string in one of the cells with respect to the selected column. Excel has got such a feature when double-clicking on the right column border it immediately enlarges / reduces the column.

 

Of course a certain method table.autoadjust(Area:<listrange>) that can be called via Simtalk should complete the request.

 

Thx.

1 REPLY

Re: Request for a column autoadjust feature in PlantSimulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Mak,

 

I agree that this would be a nice feature.

We will consider it for a future version.

 

Thanks for your input!

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.