Cancel
Showing results for 
Search instead for 
Did you mean: 

ResBlocked Statistics and object state

Valued Contributor
Valued Contributor

Hello,

 

I have a mixer named "Tank" (maybe confusing) which I am gathering statistics for. The way I am controlling the mixer is causing it to gather a lot of "Blocked"-time in the statistics despite the mixer never actually achieving a blocked state. I have checked this by issuing an observer on the mixer's attribute "ResBlocked" with a simple breakpoint inside, but the breakpoint is never triggered despite the gathered "Blocked"-statistics.

 

Is this a bug or am I doing something wrong/understanding blocked states wrong when it comes to mixers?

 

I have attached an example model which reproduces the problem.

 

I am running Plant Simulation V12.0.0

 

Thank you.

3 REPLIES

Re: ResBlocked Statistics and object state

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

install the latest patch, it is running with 12.0.2

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net

Re: ResBlocked Statistics and object state

Valued Contributor
Valued Contributor

Thank you, I installed 12.0.3 and it works flawlessly.

 

Is there an E-mail subscription where I can receive news about the newest Plant Simulation version?

 

Thank you.

Re: ResBlocked Statistics and object state

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi ET_Boys,

 

on the start page there is a tile which leads you to our Twitter channel.

 

There we post news about updates.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.