Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Retrieval procedure out of a High Bay Warehouse

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello UniStudent89,

 

you can not mix up the two libraries.If you want to use the HBW3D library, you have to adapt you methods.

 

The products are blocked because the move command of first product can not be executed because the main line 'Förderstrecke' is failed.

I would suggest to split up the main line into several short lines and use the Converter object for moving the parts from or to the in going and out going lines.Using this object it is not necessary to take care about moving parts in and out of the RSU.

 

Regards

 

GG

 

 

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Re: Retrieval procedure out of a High Bay Warehouse

Creator
Creator

 

Hello GG,

 

thank you very much for all your help. Now it's finally working Smiley Happy

 

Best Regards

 

Unistudent89