Cancel
Showing results for 
Search instead for 
Did you mean: 

Reverse sequence of production of MUs in source

Valued Contributor
Valued Contributor

Hi,

 

I am creating a model in which I have parts say A, B & C which will be produced by source according to their daily requirement, The setup change is only require when I switch processing from A or B to C and vice-verse; i.e., no setup change is required when I switch from A to B. In order to minimise the setup changes and meet the daily requirement I first produce parts in sequence A -> B -> C. After I meet firsts day reuirement for all 3 products, then, for the next day instead of starting again over with A i will start with C i.e. the sequence will be C -> B -> A.

 

So is there any way by which we can reverse the sequence of MU production at source?

1 REPLY 1

Re: Reverse sequence of production of MUs in source

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you could make a longer sequence, until the sequence is reapeating

 

A -> B -> C-->C-->B-->A for two days

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net