Cancel
Showing results for 
Search instead for 
Did you mean: 

Send MU on a assembly station within a frame

Builder
Builder

Hi all,

 

I've joined a model with my problem, there's a breakpoint on the problem.

 

I'd like, in the output of the frame named "Task_01", to send an entity on all the sucessors, except the sucessor 1 where i want to send the actual entity.

 

If I  "create" an entity on the assembly station of the Task_03, the entity will not be processed.

 

Mainly, I need a solution to send an entity on all the sucessors :

- without create a new connector

- without create a buffer at the entrance of my frame

- be sure that the entity will be processed on the assembly station where it is sent

- be sure that the "entrancecontrol" & "entrancecontrol before actions" will be executed when my new mu arrive on the assembly station

 

Any idea ?

 

Thanks a lot !

 

1 REPLY

Re: Send MU on a assembly station within a frame

Builder
Builder

Problem solved !

This seems to be because I tried to send a MU without connector on an assembly station (which need to have the information of the origin of the MU related to the predecessor, in order to know the assembly logic within...).