Cancel
Showing results for 
Search instead for 
Did you mean: 

Set the Data Type of a Column with Simtalk ?

Builder
Builder

Hi,

 

Is it possible to set the data type of a column (or create a new column in an existing table) with simtalk ?

 

Thanks in advance !

 

Flo_M

2 REPLIES

Re: Set the Data Type of a Column with Simtalk ?

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Flo_M,

 

just have a look at the method 'setDataType' of the table.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Set the Data Type of a Column with Simtalk ?

Builder
Builder

Hi ralf,

 

exactly what i needed ! Thanks Smiley Happy

 

I looked in the "help" of plant, but I was looking for "format" or something like that and didn't found setdatatype.

Are there plans to incorporate tags or synonyms in the plantsimulation help document ? I would be very helpful !