Cancel
Showing results for 
Search instead for 
Did you mean: 

SetMuTraceRouteMethod with an Attribute of Type Method

Siemens Genius Siemens Genius
Siemens Genius

Hello Forum,
I have a question regarding the SetMuTraceRouteMethod which is of an optical nature:
In a model I tried using the SetMUTraceRouteMethod which works fine as long as the method I have set is a 'method-block' in the model.

Instead, if I try using an Attribute of the type method, I get an error-message saying, that a VOID-path can't be set.

Attached you will find a modell showing this behaviour.

The version, I am currently using is V12.2.
Has anybody else encountered this problem and is there an easy fix?
As I have mentioned before, this isn't relevant for the model behaviour but I prefer the cleaner look without 'method-blocks'.

Thanks in advance.

Regards,

Tim_K

2 REPLIES 2

Re: SetMuTraceRouteMethod with an Attribute of Type Method

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Tim,

Unfortunately this method currently only supports method objects.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: SetMuTraceRouteMethod with an Attribute of Type Method

Siemens Genius Siemens Genius
Siemens Genius
Hello Ralf,
thank you for your reply. I guess, I'll just have to hide the object in some frame.
Regards,
Tim