Cancel
Showing results for 
Search instead for 
Did you mean: 

Setting up formate on subtables.

Valued Contributor
Valued Contributor

Hello Community.

I use Plant Simulation 11, educational license.

I have the odd problem, that if I create a sub table inside a table;
I cannot set the format as I wish to. The subtable will only contain Strings in its columns;
and the options to activate column and line index are grayed out;
as well as the option to right click on the header (string) and click "Format"
to change it into a time or an object for example.
On the top level table, I disabled inherit content and inherit format.

It is strange, it should be very much possible to simply edit the format;
I must have overseen something very basic. Thank you very much for answering!

Greetings

4 REPLIES 4

Re: Setting up formate on subtables.

Phenom
Phenom

0. make sure, table inheritance is switched off

 

1. select the table column

1.1 press right mouse button

1.2 select "format"

 

2. select "Tabellenformat" tab

 

3. select complete table

 

4. press right mouse button

4.1 select "format"

 

5. change subtable format

 

 

Unbenannt.PNG

Re: Setting up formate on subtables.

Valued Contributor
Valued Contributor

Thank you very much.
This was new to me ;-)

Re: Setting up formate on subtables.

Valued Contributor
Valued Contributor

Out of interest, is it possible to activate column and line indices (headers with description), too?

Re: Setting up formate on subtables.

Valued Contributor
Valued Contributor

nevermind, if I delete the old subtable entries and regenerate the subtables, I get my "headers"
thank you!