Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Setup time/importer doesn't work with Mixer and Portioner objects

Pioneer
Pioneer

Hello

 

I wanted to configure Setup time and importer for setup in model with fluids objects but no setup is done for the mixer and Portioner. Do I need to have a special configuration to have setup done for both of these objects ? (tested with version 12 and 13)

Capture.JPG

 

thanks for your support

Best regards,

Christelle

1 REPLY 1

Re: Setup time/importer doesn't work with Mixer and Portioner objects

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Christelle,

the attached model for Plant Simulation 12 is simular to your picture and ahows that setup is performed with workers. The important point is that setup is necessary when the product is changed. Because the Mixer is already prepared for the first product the first change is produced without setup.

The change of the product is modeled in the Init method.

Regards,

Peter