Cancel
Showing results for 
Search instead for 
Did you mean: 

Share transporters in different frames

Hello users and experts,

 

 

I would like to know, if it's possible use one transporter in two different tracks that are in different frames using an "Interface". I need that this transporter goes back and forth between this frames.

 

1 REPLY 1

Re: Share transporters in different frames

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Yes,  Insert into the frames interfaces for entrance and exit and connect the interfaces with the tracks, insert all subframes into a frame and connect the entrances and exits of the subframes with connectors.

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net