Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Shift calendar "not respected" in source

Creator
Creator

Hi,

 

I have created a source with Time of creation "Interval Adjust", with a constant value of 30min.

I have assigned a Shift calendar from 6:00:00 to 14:00:00 on the source.

When I run the simulation, from the starting point 00:00:00, effectively the source don't generate any MUs until 6:00:00. BUT at 6:00:00, the source generate 11 MUs, corresponding to the amount of MUS generating between 00:00:00 and 06:00:00.

How can I asked to the source to ONLY generate Mus at working hours ? (and not keep them in memory and generate them later....).

 

many Thanks,

 

1 REPLY 1

Re: Shift calendar "not respected" in source

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi Jer_N,

 

this behavior is because you have set the source to blocking.

 

Blocking means that the source remembers the points in time where a part should have produced and creates them as soon as a MU can exit the source.

 

So switching off blocking should solve your problem.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.