Cancel
Showing results for 
Search instead for 
Did you mean: 

Show current turntable position

Experimenter
Experimenter

Hello everyone,

I was wondering if there is any way to get the current position of a turntable (e.g. in degree)?

I didn't find any attribute or function which really helps dealing with this issue.

Thanks!

 

2 REPLIES 2

Re: Show current turntable position

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

you are right, there is no such attribute. For what reason do you need this?

 

Kind regards

Karola

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Show current turntable position

Experimenter
Experimenter

Hello,

I want to create a trace file which shows the exact position of the turntable at the moment I'm aksing for it.

 

Kind regards

Jan