Cancel
Showing results for 
Search instead for 
Did you mean: 

Showing acceleration in Worker

Hello Everyone,

 

I am using the worker to simulate a robot in my model. I was wondering if there is any way to show acceleration in the worker since there is no option avilable in the worker attributes.

 

is there some other unconventional tricks i can use to do that ? does anyone have faced similar situation?

 

Thanks in advance!!

1 REPLY

Re: Showing acceleration in Worker

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

you can look up the speed of a worker, which is a constant attribute that you have to predefine, but the worker does not have an acceleration like the transporter has. So in case that you don´t need your robot to be able to move freely in your model you can use a transporter moving on tracks instead of a worker. This way you will also have the option of setting and showing its acceleration.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution