Cancel
Showing results for 
Search instead for 
Did you mean: 

Simulation of Workers

Pioneer
Pioneer

Hi,

I have a question related to workers. I am simulating a manualo assembly line and I want that the workers stays at the same station DURING the task is being performed. He can only leave the station after the operation has been finished. Can anyone kindly help me with this ?

 

Thank you in advance.

4 REPLIES 4

Re: Simulation of Workers

Experimenter
Experimenter

Hallo Niks,

Greetings From Yadav here.

Go through the syntax Workerstayshere in helpSmiley Happy

Regards,

Yadav

Highlighted

Re: Simulation of Workers

Pioneer
Pioneer

Hi Yadav,

Thank you for your kind relp. The syntax says "Worker stays here after completing the job" which means the worker will not move to the workerpool. What I exactly want is:

[1] Worker pickups the part from buffer, brings to the work station.

[2]Performs the operation and while performing the operation, he stays there only.

[3]After, completing the operation, he picks up the part and put it back to another buffer.

Point [2] is giving me trouble.

 Regards,

Niks

Re: Simulation of Workers

Experimenter
Experimenter

Hallo Niks,

can you upload reference model ?

regards,

Yadav 

 

Re: Simulation of Workers

Pioneer
Pioneer

Hallo Yadav,

Kindly find the model in the attachment. I want to simulate the worker in a way such that after picking up the part from Buffer 1, the worker stays at the work station during the operation is being performed. After the operation is finished, he delivers the part to Buffer 2 abd only after that, he goes to buffer 1 for picking up the new part.

 

Regards,

Niks