Cancel
Showing results for 
Search instead for 
Did you mean: 

Simultaneous failures at two processing table of a machine

Builder
Builder

Hello Community,

 

I am modelling a machine that has 2 processing table. I am using single procs to show table 1 and table 2. The problem is setting up the failure of the machine . In reality the complete machine is failed whenever there is a failure but in simulation model, single proc 1 and single proc 2 is failed at different time. In reality both the table should stop working in the case of failure simultaneously. How I can program the model so that both the table (single proc is failed at the same time).

Any help is appreciated ?

2 REPLIES 2

Re: Simultaneous failures at two processing table of a machine

Phenom
Phenom

Have a look at the LockoutZone object.

Re: Simultaneous failures at two processing table of a machine

Builder
Builder
Danke!! Was completely unaware about this. It will solve my problem..