Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

SingleProc use ShiftCalendar

Valued Contributor
Valued Contributor

as below shown ,a worker  services a SingleProc,the worker and SingleProc has same working utilization,however when I set   ShiftCalendar for the worker and   SingleProc,their  working utilization  are not same 

how should i solve  it 捕获.PNG捕获1.PNG

 

1 REPLY 1

Betreff: SingleProc use ShiftCalendar

Gears Phenom Gears Phenom
Gears Phenom

You need to look at the Exporter-statistics of the Worker, too!

grafik.pnggrafik.png

The statistics on the left side are relative to the Exporter-Operational part on the right side, so Paused/Unplanned is not included. In my example, the worker was working 100% of the 58.3% of the time that he was operational, so in total he worked 58.3% of the simulation time and that matches the SingleProc-statistics.

Regards,
Alex

___________________________________________________________
Alex Dilg, Consultant at SimPlan AG (www.SimPlan.de)
This post was good and/or helpful to you? Please provide some Kudos, thank you!