Cancel
Showing results for 
Search instead for 
Did you mean: 

Source set up

Hello everybody. 

I want to make a source, that will produce 33 000 pcs, after that will stop for 1h and 20 min (for changing the coil of material). It will repeat this at every produced 33 000 pcs. I know it is something easy, but i can not find the solution. 

 

Thank you in advance for the help!

 

3 REPLIES 3

Re: Source set up

Phenom
Phenom

It is probably easier to place a singleproc object after the source object

 

There you can set a setup

 

Have a look at setup time ( time tab)

 

and setup (setup tab)

Highlighted

Re: Source set up

Thank you very much for the answer. I was thinking to do it that way, but i was curious if there is another way to set the sorce. I think the only way is a long programming of the source.... I guess i will use the easiest solution. 

Re: Source set up

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

You could also set MU Selection to Sequence Cyclical, and specify the batch-size in the required table (hint: dropping a tablefile onto the Source will do the formatting for you). Also check the Generate as batch option. Set Interval to the time you want.


Gert Nomden
Digital Factory Consultant
cardsplmsolutions.com