Cancel
Showing results for 
Search instead for 
Did you mean: 

Spatial Constraints

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hey everyone,

 

I'm looking to create a model that would include spatial constraints for products/buildings/workstations. Does Plant Simulation take this into account at all? If so, where can this be implemented? For example: I don't want a part to go to a workstation that it cannot fit in.

 

Thanks

1 REPLY 1

Re: Spatial Constraints

Valued Contributor
Valued Contributor

Hi Csadler,

 

There is a way to solve this problem. You can use the user-defined attributes to define the values, which describe the entity size and the workstation space. In the entrance control of workstation, the values are being compared. If the entity size smaller than the workstation space, it can enter the workstation. Otherwise, it cannot.

 

I hope the attachment can help you!

 

Best regards!

 

 

Tao Yifei