Cancel
Showing results for 
Search instead for 
Did you mean: 

Special sequence

Pioneer
Pioneer

Hello dear community,

 

I need some help with a model I am working on. I have a straight production line with four machines (same type). The MUs must be processed in this order: MU1 enter in machine 4, MU2 in machine 3, MU3 in machine 2 and MU4 in machine 1. And so on, every four pieces.

 

So far I have tried an exit method for each, but I am not sure how to identify the number of MUs in order to write the condition in the method.

 

Thanks in advance!

 

 

Unbenannt.png

2 REPLIES

Re: Special sequence

Valued Contributor
Valued Contributor

Hello IImartinez37, 

 

maybe you can try it like this Capture.PNG

 

so there is an variable that counts the MU`s. If the 4th MU comes to the exit it will be moved to the other line. 

 

regards, 

 

david 

 

 

Re: Special sequence

Genius
Genius

Hello llmartinez,

 

Please make use of Destination attribute of MUdestination to MUs1.PNG

 

 

 

 

 

 

 

 

 

And update the exit strategy of the conveyorsdestination to MUs.PNG

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Please refer the attached model for your reference.

 

Thanks & Best Regards,

Abhilash S.

 

 

Thanks & Best Regards,
Abhilash Sridhar
Mercedes Benz R&D India, Daimler AG