Cancel
Showing results for 
Search instead for 
Did you mean: 

Starting with filled line

Valued Contributor
Valued Contributor

I want to simulate a case study with all buffers filled with 10 MUs at start. What method sould I use to do the same?

 

 

Also is it possible to produce 1 MU on each single processing Unit?

1 REPLY 1

Re: Starting with filled line

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

you could use an init-method in the buffer (as user defined attribute). In this init-method you can create the parts, e.g.

 

is 
i:integer;
do
for i:=1 to 10 loop
.MUs.Entity.create(self.~);
next;

end;

In the same way you can create MUs on SingleProcs (see help: create) 

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net