Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Station Failure query

Creator
Creator

Greetings,

 

I have a model which has 5 stations connected and all the stations have same failure data.

However I want them to fail at different point of time and not at the same time. The model runs for one year.

 

MTTR and availability is same for all stations. Only the time of failure needs to be different.

 

Is it possible to have random stream or number generated for each station failures?. 

 

Thanks in advance.

 

Regards,

Aravind

1 REPLY 1

Betreff: Station Failure query

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Aravind,

 

by default, all stations in Plant Simulation have different random number streams and therefore the disruption of every station will start at a different time. This will be shown, when you open the event list of the EventController after pressing Reset and making one single step (see attached screenshot)

Failure.jpg

Hope this helps

 

Regards

GG

 

 

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution