Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Step/Maintenance work on Workstation (SingleProc)

Legend
Legend

I know this setup, it happens before the process time.

Our setup (real world) shall happen every x hours of process time on the station.

 

I cannot set it as the importer part is disabled/greyed out.

The failure allows me to setup the first start time, any further start time and duration.

 

 

Re: Step/Maintenance work on Workstation (SingleProc)

Phenom
Phenom

If I remember well, your question was :

 

What is the correct way to implement service/maintenance in the plant simulation ?

 

The correct way to define set-up in Plant Simulation is to use the set-up features provided

 

by Plant Simulation.

 

The Set-up ( in real world) usually depends on the number of produced parts during production

 

time not solely on a  predefined maintenance period.

 

E.g. welded spots in Body in White production.

 

From the cycletime ( per part) and your time until setup , you can calculate the part count

 

input parameter for Set-up in  Plant Simulation.

 

Switch off common resources and you can set the the set-up importer( s.b.)

 

In any case if you want to use the fixed set-up periods you can always

 

use the "failure" solution.

 

Unbenannt.PNG

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

Re: Step/Maintenance work on Workstation (SingleProc)

Legend
Legend

I guess I will try it out and use the setup after number of parts. I can calculate this using the known process time.

 

Thanks