Cancel
Showing results for 
Search instead for 
Did you mean: 

Still missing time for resource utilization portions

Creator
Creator

Hello,

 

I do not know if I understand well the resource statistics, because I thought that these resource statistics percentages should add to 100 but it is not the case (see attached image).

 

Please can someone help me to understand what is happening ?

(Attached a simple model showing the issue)

 

I've read an other topics with kind of same issue but siemens user said it will be fixed in version 13.2, i'm currrently using version 14.0.

 

Thank you in advance.

5 REPLIES 5

Re: Still missing time for resource utilization portions

Creator
Creator

Re: Still missing time for resource utilization portions

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

for me the statistics add up and look a bit different in your model using version 14.0, see the attached picture. At what point of time do you look at the statistics? What also often helps in such cases is to refresh the window by pressing F5 to see the actual statistics at that moment.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Still missing time for resource utilization portions

Creator
Creator

Hello Igor,

 

Thank you for your reply.

I'm looking and refreshing the statistics at the end of the simulation (2480 entries). And I do not have same statistics as you (where statistics add to 100).

Wich version are you using ? (I'm on the 14.0.1.1207)

 

 

 

Re: Still missing time for resource utilization portions

Creator
Creator

Hello again,

 

And for me, the total should always be 100, no matter when we look at the statistics.

 

BR,

 

Clément.

Re: Still missing time for resource utilization portions

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Clement,

 

I see this is indeed a bug in your version which was already fixed. If you install a newer maintenance pack this issue should disappear.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution