Cancel
Showing results for 
Search instead for 
Did you mean: 

Stopping the full cycle time of a processed part through a production line

Valued Contributor
Valued Contributor

Hello, dear community, engineers, and experimenters,

 

I am looking for an efficient and straightforward way how to count time on an MU from the first entry of the production line until being sent to the output storage (Ausgangslager).
I thought about an user-defined Attribute and maybe using a sensor;
but currently all MUs are moved via method, not transportation path, so I am not sure how to place the sensor;
OR how to write this in a method in the exit strategy of the source and the entry strategy of the output storage to call this timer and to stop it again (and return the value on a list).

 

thank you very much for your hints!

 

1 REPLY 1
Highlighted

Re: Stopping the full cycle time of a processed part through a production line

Legend
Legend

I had a similar requirement last week. You can define user-defined attributes of data type 'time' in the main MU class. 

(maybe name them IN_time and OUT_time) 

 

Assign the value to these attributes in entry or exit controls as you already understand.

You can do something like the following...

 

At the first entry into the production:

@.IN_time := root.EventController.SimTime

At the exit towards output storage:

@.OUT_time := root.EventController.SimTime

Once you have these values, you can record them in a table.

 

The difference between the OUT_time and the IN_time will be the total time that the part spent in the production area.

 

 

To add it to a table, create a table in the frame(myTable) and add rows for each MU.

myTable.appendRow(@.Name, @.IN_time, @.OUT_time, (@.OUT_time - @.IN_time))

Hope this helps.