Cancel
Showing results for 
Search instead for 
Did you mean: 

Struggling getting Microstation files into Plant Simulation

Siemens Experimenter Siemens Experimenter
Siemens Experimenter

Hi all from Down Under.  

 

We are struggling to a customers DNG file format into Plant Simulation.

 

Failing not being able to import DNG directly into Plant Sim as there is not direct interface. As an alternative we have gone down a path of IGES which only exports curves only. STEP which crashes Microstation during export and we also tried Parasolid XMT/X_T for which their systems can't produce the file.

 

For STEP we have no idea. For Parasolid, it's likely they don't have licences for Parasolid. 

 

They have been able to export and import a Wavefront OBJ file successfully at their end. 

 

Is there any way to get OBJ file format into Plant Simulation?

 

Thank you.

Hakan

 

In the mail Matthew did not mention jt export. Did they try? We had Bentley Microstation at FSG as well and jt export worked quite fine.

 

2 REPLIES 2

Re: Struggling getting Microstation files into Plant Simulation

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Hakan,

You can import a DGN file as a textured plate into 3D.

Have you tested this?

 

An alternative would be as you said to write a JT from MicroStation.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Struggling getting Microstation files into Plant Simulation

Phenom
Phenom

a further alternative is the VRML2 export from microstation and  import to Plant Simulation which

 

usually always works.