Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Subframe in Shift Calendar Resources

Hello,

 

Is there a difference between adding a whole subframe to the objects list in the Resources tab of the model's Shift Calendar or adding each station from the subframe individually?

 

Thanks!

1 REPLY 1

Re: Subframe in Shift Calendar Resources

Phenom
Phenom

Hi @Pedro_Manfroi 

 

If you add the subframe as you said, the frame will trigger its Pause and Unplanned controls. Then, you can do whatever you want plus pausing stations (recreating what you observed). For instance, imagine a situation where you just pause a machine if the remaining processing time is higher than a particular time. Using pause methods on a subframe would be a way to solve that. Take a look at this section of the documentation, there is a nice example there:

 

shiftcalendar.PNG

Best Regards,
Paulo Araujo

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.