Cancel
Showing results for 
Search instead for 
Did you mean: 

Take material from the buffer before process

Creator
Creator

Hello,

 

What code should I put in entrance of Assembly Station to take material from the buffer when it is waiting for main MU?

Like in simulation below: station "Panel" could take MUs from Buffer. Now first it is waiting for main MU prom predecessor.

ps1.jpg

1 REPLY
Highlighted

Re: Take material from the buffer before process

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
the entrance of the assembly is the wrong place, best way is not to use an exit control in the buffer, so that the buffer is moving the main part to the assembly station. Alternatively you can use an exit control in the buffer: wait until panel is empty and move the part:

waituntil panel.empty
@.move(panel)

Steffen Bangsow
freelance simulation specialist  
web: www.bangsow.eu
mail: steffen@bangsow.net