Cancel
Showing results for 
Search instead for 
Did you mean: 

Tecnomatix Plant Simulation 11.0.1 released!

Siemens Phenom Siemens Phenom
Siemens Phenom

The first patch for Tecnomatix Plant Simulation 11 was released.

 

You can download it here: http://ftp.ugs.com/tecnomatix/Plant_Simulation/Patches/Version_11.0/

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.
6 REPLIES 6

Re: Tecnomatix Plant Simulation 11.0.1 released!

Community Manager Community Manager
Community Manager

Please be aware that when installing this patch you will see an erroneous message at the end of the install referring to version 10.1.1 (see below).

 

Tecnomatix Plant Simulation Update_2013-06-28_09-43-56.png

 

Do not be bothered by this and rest assured that the 11.0.1 version was successfully installed.  You can verify this by loading Plant Simulation and checking the installed version through the Help menu.  This is a known issue and it will be corrected in the next patch release.

 

Mike Rouman
Senior Marketing Manager
Manufacturing Engineering Software
Siemens Digital Industries Software Inc.

Re: Tecnomatix Plant Simulation 11.0.1 released!

Experimenter
Experimenter
i cannot download the plant simulation 11. please provide me a direct download link. thank you.

Re: Tecnomatix Plant Simulation 11.0.1 released!

Siemens Phenom Siemens Phenom
Siemens Phenom

The installation can be downloaded here:

Full Product Download: https://download.industrysoftware.automation.siemens.com/download.php

 

Updates for Tecnomatix Plant Simulation 11 can be downloaded here:

Updates: https://download.industrysoftware.automation.siemens.com/tecnomatix/Plant_Simulation/Patches/Version...

 

You have to use your Webkey to login.

Here you can find a description on how to obtain a Webkey: Webkey: https://plmapps.industrysoftware.automation.siemens.com/webkey/

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Tecnomatix Plant Simulation 11.0.1 released!

Experimenter
Experimenter
unable to open my webkey. please provide easy access link to download plant simulation 11 or plant simulation 10 full version.

Re: Tecnomatix Plant Simulation 11.0.1 released!

Siemens Phenom Siemens Phenom
Siemens Phenom

This is the only official way were you download our software.

 

if you have problems please contact our GTAC support organization:

http://support.industrysoftware.automation.siemens.com/gtac.shtml

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Tecnomatix Plant Simulation 11.0.1 released!

Legend
Legend

These kinds of postings are great, along with the twitter updates! Any plans on pinning posts about the current patch release in the top of the forum?

 

Also, what is your stance on posting the patch notes? Is that considered sensitive data? Could be another thing to include when doing a post like this.