Cancel
Showing results for 
Search instead for 
Did you mean: 

Tecnomatix Plant Simulation 13 Windows server

Experimenter
Experimenter

Hello,

 

I would like to install Tecnomatix Plant Simulation 13 on the cloud. Will I be able to install a runtime licence and the licencing software on a virtualised Windows Server OS and, if so, which versions of Windows Server are supported? Ideally I would be able to use Windows Server 2016.

 

Many Thanks.

1 REPLY 1

Re: Tecnomatix Plant Simulation 13 Windows server

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello CJD,

As long as you configure your Firewall so that it doesn't block it should work. The relevant ports are 28000 and the vendor port which you have to define yourself on the VENDOR line of the license file:

e.g. VENDOR PORT=28100

The license server should work fine on Windows Server 2016.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.