04-19-2017 11:24 AM
Dear Plant Simulation users,
Plant Simulation version 13.2 has been released and is published and available on the
Siemens PLM Software GTAC server.
The new version is the second mile stone and step towards the major release of version 14.0 in August 2017. The new 13.2 Plant Simulation release comes with enhanced material handling capabilities and a powerful new approach for virtual commissioning in combination with PLCSIM Advanced, the virtual S7-1500 PLC controllers of Siemens:
As always you will see several additional enhancements in the What's New chapter of the online help.
Please have a look for further details there!
All users with active GTAC account are invited to explore,
use and enjoy the new Plant Simulation software!!
Best regards
gepi
04-20-2017 02:23 AM
06-28-2017 08:29 AM
Hello gepi,
is it already possible to download or update to version 13.2 with a student license?
Best regards,
KilianV
06-30-2017 09:21 AM
Hello Kilian,
the Plant Simulation minor versions are intermediate releases towards the final major versions.
Today we have 13.1 and 13.2 as steps towards version 14.0, planned for end of August 2017.
A while after release of version 14.0 this version will also be used for the student download.
I am afraid you need to wait :-( for the latest developments for being accessible through the student program.
Best regards
gepi
06-30-2017 09:34 AM
08-01-2017 09:02 AM
What is going wrong if I can't find the version on the GTAC server?
08-01-2017 09:43 AM