Cancel
Showing results for 
Search instead for 
Did you mean: 

Texture to objects

Pioneer
Pioneer

Good morning, I would like to put an image as texture of an object. For example to put this image 

imagen.jpg

 

in the face of this object

duda.png

 

I have tried to import the solid in .jt from NX 10 with the image but the solid doesn't appears with the image. Any solution?

 

Thank you

1 REPLY 1

Re: Texture to objects

Siemens Phenom Siemens Phenom
Siemens Phenom

Have you tried to create a textured plate?

You can do that by going to the 3D Edit ribbon, there selecting the entry "Textured Plate" from the "Insert Shape" group and loading the picture you want to use as texture.

You can specify the orientation of the plate so that you can create a textured wall (not only a floor plate), too.

Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution