Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: The maximum number of call-chains was exceeded

Creator
Creator

Hi guys,

 

So far I could not follow. So was was the actual solution to avoid this error message in version 14.

I am facing the same error thrown "the maximum number of call-chains was exceeded" even for a small condition query like 

 

if not SingleProc.empty then

    .....

else

   ......

end

 

So the error is thrown already for the first condition check. How can I avoid that issue?

Thanks for your help!

 

Best regards,

 

Timbo

Re: The maximum number of call-chains was exceeded

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Timbo47,

 

Just have a look on the tab Call Chains in the debugger to understand why you have so many call chains.

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: The maximum number of call-chains was exceeded

Genius
Genius
Hello,Ralf
Could you spare your valuable time to look at the Topic:
the thread is shown in the following picture:
https://community.plm.automation.siemens.com/t5/Plant-Simulation-Forum/How-to-deal-with-the-LOGIC-of...