Cancel
Showing results for 
Search instead for 
Did you mean: 

Tomáš - I need help

Experimenter
Experimenter

Good morning

I am student on Technical University and Can you help mi with one project in school.

I invented one matematic model for Transporter and i need to try it. But my skill in Plant Simulation is realy low. I need made Model like in annex.

If you have same question this is my email: tomas.torok@gmail.com

When you can hepl me, I will pay you

Thanks

7 REPLIES

Re: Tomáš - I need help

Legend
Legend

Hello Tomas,

it is quite impossible to understand what you want to do by your image.
If you provide a description we will help you.

Alessio

Re: Tomáš - I need help

Experimenter
Experimenter

Hi 

I need to put two transporter in  simulation. I use transfer station for load, unload but i do not know it is good.
Can you help me with insert Transporten in simulation
Thank you
 
And second step 
I need hepl with Metod - where go to Transporter
I have matematic model. How to decide transporter Bat i do not insert
Becouse i neet to using Signal level in buffer

Re: Tomáš - I need help

Legend
Legend
I don't know how to help you without knowing what you are trying to model.

Can you explain the process?

Transfer stations are ok to load parts from a station to the transporter and viceversa.
The transporter has an attribute called destination which could be useful to send it to a specific position.

Re: Tomáš - I need help

Experimenter
Experimenter

I do not how insert Transporters in simulation Because i am beginner in this software

i sent you my material flow

 

Re: Tomáš - I need help

Legend
Legend

I understand a bit more your system now.
Still there is not any information about the transporter logic. Are there priority? How does the transporter decide where it must goes when several missions need to be performed?

Re: Tomáš - I need help

Experimenter
Experimenter

 

Truck must know where they are (near witch machines). 

I need , if you knew me show methods - Call transporter to buffer, acording to the signal level in buffer.

And help me make transporters in this model

 

 

Then i try learn transporter how choose one of the options of transport, this i try make own

 

Thanks for your time

Re: Tomáš - I need help

Legend
Legend

Hi,
I made a small model with a simple logic.

Basically there is a transporter which performs different missions:

- when a part arrives at the "load bay", it brings the part to the buffer with less entities (if no buffer is available the mission in postponed)

- when a buffer reaches the threshold the transporter brings all the parts contained to the "unload bay".

The code is not optimized, but is a start for you to create your own model.

Just a warning: this example could be event too much complex for your needs, so think first what exactly you need to model.

Regards
Alessio