Cancel
Showing results for 
Search instead for 
Did you mean: 

Tool changeover frequency method

Valued Contributor
Valued Contributor

Hi everyone

 

I need a logic where i have n number of machines connected in series and each of these machines after processing say n number of parts individually, requires a tool change over because of the worn out conditions of the tool and this changeover of the tool may require x seconds and this changeover time differs from machine to machine.

 

Thanks and Regards

Sujith

3 REPLIES 3
Highlighted

Betreff: Tool changeover frequency method

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello Sujith123,

 

on tab Set-Up you can select strategy 'After n parts'. On tab Times, you have to define the set-up time. You can use a constant set up time or any distribution function.

 

Regards

 

GG

Regards
GG

------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution

Betreff: Tool changeover frequency method

Valued Contributor
Valued Contributor
Hello

I tried this, if i use this logic and specify the setup time and make the
model run, the single proc remains idle for x minutes right at the start of
the simulation when the first entity enters though the settup strategy in
the setup tab is selected as n parts and after last part.

Kind Regards
Sujith

Betreff: Tool changeover frequency method

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi Sujith123

One way to go around the first set-up is to use the following code in an init method:

 

singleProc.setupTime:=str_to_time("1")
singleProc.setupfor(.MUs.Entity)
singleProc.setupTime:=str_to_time("1:00")

 

You do this for each SingleProc. It is not pretty but it works Smiley Tongue