Cancel
Showing results for 
Search instead for 
Did you mean: 

Track 3D icon

Legend
Legend

Hi guys

in my model sometimes I need to create the 3D layout of the plant. To do that I use a .jt file and I insert it in my objects (i.e. in a frame for my machining centers).


The problem is modify the 3D icon of length oriented objects such as tracks. I can change the icon, but when I modify the  length, the previous icon (the standard one) reappears.

Is it possible to use a jt or another 3D file to model this objects? If so, how can I proceed?

Thank you!
Alessio

 

4 REPLIES

Re: Track 3D icon

Phenom
Phenom

you can add another graphic

and

you can switch off the 3d default graphic

 

Unbenannt.png

 

Re: Track 3D icon

Legend
Legend
Thank you Simulator.

If I haven't done any mistake, in this way I see the imported graphic, but it doesn't change its length according to the length of the track.

Re: Track 3D icon

Phenom
Phenom
if you have to adapt the size/ length of an individual supplemental graphic object,
you can manually scale it in x-, y-,z direction.



Re: Track 3D icon

Legend
Legend
That could work, I will try.
Thanks for the tip.