Cancel
Showing results for 
Search instead for 
Did you mean: 

Track with Sensors

Good Morning!

 

I would like to make a track using these sensor possibilities.

 

Picture in the attachments

 

I'm new to Plant Simulation.

 

Thank You.

6 REPLIES

Re: Track with Sensors

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello,

 

here is a model attached that should implement something similar what is in your picture. You can set the vehicle to start and stop at the designated positions with the global variables in the frame.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Track with Sensors

I can not open this template.
my version of plant simulation is 13.2

 

Thank You.

 

Kind regards,

 

Matheus Ferraz

 

Re: Track with Sensors

Siemens Phenom Siemens Phenom
Siemens Phenom

You should now be able to open the model. Whenever the vehicle stops you can make it continue driving on the track by running the Start_vehicle method in the frame.

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Track with Sensors

How do I make a full turn and then stop at sensor1?

which method do I write?

 

Equal these possibilities in the image of the annex

 

Thank You!

 

Kind regards,

 

Matheus Ferraz

Re: Track with Sensors

Siemens Phenom Siemens Phenom
Siemens Phenom

Attached is the model with the function to loop through all of the possibilities described in the list file, stopping at the respective sensors and the stop position in every round for a short while. After all possibilities are looped through, the vehicle stops at the stop position. The time that the vehicle waits at a station and at the stop before continuing to drive can be designated in the variable "Waiting_Time".

Kind regards,

Igor
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution


Re: Track with Sensors

Thanks for your help!!!
You are the best =)

 

Regards,

 

Matheus Ferraz