Cancel
Showing results for 
Search instead for 
Did you mean: 

Transfer n-MUs to Worker at once

Creator
Creator

Hello.

 

Just a quick question. I´m trying to model the following behavior:

  • Worker is called when >=5 MUs are in the buffer
  • Worker grabs 5 MUs at once -> How can I program this?

Any help would be appreciated.

 

3 REPLIES 3

Re: Transfer n-MUs to Worker at once

Phenom
Phenom

acc. to your model, the worker is already grabbing 5 MuUnbenannt.pngs

 

Re: Transfer n-MUs to Worker at once

Creator
Creator

Sorry, looks like didn´t explain myself well.

 

The problem is, that the worker waits too long.

 

At the Moment it is like this:

  • Timecode: 5:00 - 5 MUs are in the buffer, Worker is dispatched and grabs first MU
  • Timecode: 5-9:00 - Worker waits and grabs a MU every minute
  • Timecode: 9:00 - Worker walks away with 5 MUs


I want something like:

  • Timecode: 5:00 - 5 MUs are in the buffer, Worker is dispachted, grabs 5 MUs from buffer and walks away

Re: Transfer n-MUs to Worker at once

Phenom
Phenom

try it with this slightly modified methodUnbenannt.png