Cancel
Showing results for 
Search instead for 
Did you mean: 

Transfer station will not let MU's pass

Hi All

 

I have a line with Entitys on it. I want to take one Entity form the line and process it in a SingleProc, when the Entity is done I want to put it back to the line, when there is space.

 

While I am processing one part the rest of the Entity should continue on the line (to the next station) so it can be procesed on an other station.

 

I have tryed to use a TransferStation but how do I avoid that it is blocking all the rest Entitys on the line. I have set the station type to "Move" and under Advanced Attributes the check box "Always stop container" is greyed out.

 

If you have an other idea to solv the problem let me know to.

 

 

Thanks
Kind Regrads

2 REPLIES

Re: Transfer station will not let MU's pass

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi,

 

you can use a sensor control to put the entity onto the station:

 

Just write something like the following into your sensor control:

	if SingleProc.cont = void then
		@.move(SingleProc);
	end;

 

So create a sensor for each station and then use the TransferStation to put the entity back onto the line.

 

Regards,

Ralf

Regards,

Ralf
------------------------------------------------------------------------------------------------------
Did you like the answer? Then click the Thumbs Up button.
Did the answer solve your problem? Then accept the answer as solution.

Re: Transfer station will not let MU's pass

Hi Ralf

Thanks for tha fast answer.

 

It worked like a charm.